Pulse Building

Importing Settings from a CSV File

In the Pulse Building application, you can import the following settings from Comma-Separated Values (CSV) files:

Pulse Types - The Import option is applicable for the following pulse types.

Modulation Settings - The Import option is applicable for the following modulation types.

Hop Patterns - The Import option is applicable for the following Hop pattern type.

Antenna Pattern - The Import option is applicable for the following Antenna pattern type.

PRI Pattern - The Import option is applicable for the following PRI pattern type.

To import settings from a CSV file

This procedure uses the example of importing modulation settings. Similarly, you can import other settings from a CSV file.

  1. Got to Pulses > Modulation tab.

  2. Select a Modulation Type that supports importing settings from a CSV file.

  3. Click the button to display the menu for configuring modulation settings.

  4. Click the Import option from the displayed menu.

  5. Navigate to your modulation settings csv file and click Select.